S32 install on win7 - problem?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 install on win7 - problem?

4,942 次查看
evian
Contributor II

Have tried to install S32_Design_Studio_for_ARM_v1.2 for windows on two win7 set-ups on different networks and always get the same error in the log file. Has anyone found a solution?

 

Make Registry Entry:      Key: HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\Uninstall\S32 Design Studio for ARM v1.2
                          Value Name: Comments
                          Value Data: Automotive S32 Design Studio v1.2
                          Status: SUCCESSFUL

Install Uninstaller:      S32 Design Studio for ARM v1.2(Install All Uninstaller Components)
                          Status: ERROR
                          Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

4 回复数

4,371 次查看
martin_kovar
NXP Employee
NXP Employee

Hi,

please look at the following thread:

How to uninstall S32DS for ARM v1.1

We have already solved similar issue.

If it does not help you, please write me back a I will try to find another solution.

Regards,

Martin

0 项奖励
回复

4,371 次查看
evian
Contributor II

I have now resolved this by using another activation code. There seemed to be a problem with the original code supplied

4,192 次查看
zz20102007
Contributor I

I encountered the same problem when installing S32 v1.2. How did you solve it?

0 项奖励
回复

4,168 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @zz20102007,

I checked your account, there is no record of any activation attempts. What activation code are you using? Please check that it is the one that is matched with the product you are trying to activate.

Best Regards,

Mike

0 项奖励
回复