S32 generates PTP format output with diab compiler installed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 generates PTP format output with diab compiler installed

1,677 Views
Nxp_2022
Contributor I

Hello,

I tried to compile a project with diab compiler installed in S32, and wanted to generate PTP binary format other than elf default output.

How can I configure S32 and set up compiler option to make this happen?

Thanks for your time! 

-Jim

0 Kudos
Reply
4 Replies

1,638 Views
jiri_kral
NXP Employee
NXP Employee

Hi Jim, 

I don't have installed Diab plugin - but you may find helpful this thread https://community.nxp.com/t5/S32-Design-Studio/DIAB-generate-binary/m-p/1237940/highlight/true 

 

You can add the ddump.exe command to post-build steps - this option should be somewhere in project properties. 

0 Kudos
Reply

1,650 Views
Nxp_2022
Contributor I

Thanks Lukas,

As my project is working with installed diab compiler, there is no option about flash image available under "C/C++ build -> Settings", I also looked over the others, but didn't find any binary output setting. I am wondering should I need to do anything in "Diab C Linker" section under Other tab in following screen shot, and what kind of option has to be applied?

Best regards,

-Jim

Nxp_2022_0-1677603172380.png

 

 

0 Kudos
Reply

1,643 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Jim,

ok, I have never had Diab plugin installed... @jiri_kral would you know if Diab support this?

Regards,

Lukas

0 Kudos
Reply

1,658 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport
0 Kudos
Reply