S32 design studio v1.1 debug error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 design studio v1.1 debug error

3,005件の閲覧回数
李国宁
Contributor I

When I debug my MPC5744P demo code with PE in S32 design studio, the progress bar increase to 98% then can not finish debugging. There is errors in the console window of S32 design studio, as the following figures shown. Can anyone help me? Thanks very much.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,799件の閲覧回数
jianweiwu
Contributor I

Hello Gavin,

I met this problem too,could you please tell me how to solve it ?Thanks very much.

0 件の賞賛
返信

2,799件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Gavin,

This error indicates a debug connection issue with your board.

Could you try to create an empty project for MPC5744P using project wizard build it and debug it?

You can try to switch to Debug_RAM build configuration first to make sure you are able to load the RAM first.

Stan

0 件の賞賛
返信