S32 design studio open fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 design studio open fail

4,329 Views
chih-hsihsu
Contributor I

Hello, NXP Team

When I click the S32 design studio, it will show "An error has occurred.See the log file" and then the configuration folder will be created log document which is record some error information in there.

So, How could I solve this problem? 

Thanks and Regards,

CHIH-HSI

0 Kudos
Reply
5 Replies

4,100 Views
chih-hsihsu
Contributor I

HI Jiri,

I follow your recommendation to delete the file but it's still doesn't work.
when click the s32ds,the message show the same things that I mentioned before.

Regards,

Chih-Hsi

0 Kudos
Reply

4,099 Views
jiri_kral
NXP Employee
NXP Employee

Hi Chih-Hsi,

I checked again you log file - and the keylock issue is probably related to osgi container only. Please try to delete .FileTableLock file from this directory:

[Your S32DS install path]\S32_Power_v1.1\eclipse\configuration\org.eclipse.osgi\.manager\

Jiri

0 Kudos
Reply

4,099 Views
jiri_kral
NXP Employee
NXP Employee

Hi Chih-Hsi,

Your issue is probably related to known eclipse Bug 472108. You can try to delete .FileTableLock file located on

[Your S32DS install path]\S32_Power_v1.1\eclipse\configuration\org.eclipse.core.runtime\.manager\ 

You can delete all files in this directory. Also make sure that you have rights for writing into this directory. 

Jiri 

0 Kudos
Reply

4,099 Views
chih-hsihsu
Contributor I

Hello, NXP team:

The S32DS is 1.1 version power and operating system is windows seven

Ok, please follow attachment.

0 Kudos
Reply

4,099 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

Could you please clarify following points?

  • Which S32DS you use? ARM or Power? Which version?
  • Which operating system you use?
  • Could you please share the log file?

Regards,

Martin

0 Kudos
Reply