S32 design studio for power architecture version 2017.r1 compiler optimization level O1, what specif

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 design studio for power architecture version 2017.r1 compiler optimization level O1, what specif

Jump to solution
2,350 Views
StarMao159376
Contributor II

Hi,Sir, S32 design studio for power architecture version 2017.r1 compiler optimization level O1, what specific optimization has been done, and can optimization be enabled?

Found in the actual project: 1 For the same 200m main frequency, mpc5744 takes more than twice as long as tc275!!!

2. However, when the optimization above O1 is enabled, the operation efficiency is significantly improved

0 Kudos
Reply
1 Solution
2,331 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

 

s32ds uses gcc compiler - the optimization level description you can find here: 

https://gcc.gnu.org/onlinedocs/gcc/Optimize-Options.html

 

Jiri

View solution in original post

0 Kudos
Reply
2 Replies
2,332 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

 

s32ds uses gcc compiler - the optimization level description you can find here: 

https://gcc.gnu.org/onlinedocs/gcc/Optimize-Options.html

 

Jiri

0 Kudos
Reply
2,311 Views
StarMao159376
Contributor II

Thanks.

0 Kudos
Reply