S32 design studio for power architecture version 2017.r1 compiler optimization level O1, what specif

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32 design studio for power architecture version 2017.r1 compiler optimization level O1, what specif

跳至解决方案
2,430 次查看
StarMao159376
Contributor II

Hi,Sir, S32 design studio for power architecture version 2017.r1 compiler optimization level O1, what specific optimization has been done, and can optimization be enabled?

Found in the actual project: 1 For the same 200m main frequency, mpc5744 takes more than twice as long as tc275!!!

2. However, when the optimization above O1 is enabled, the operation efficiency is significantly improved

0 项奖励
回复
1 解答
2,411 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

 

s32ds uses gcc compiler - the optimization level description you can find here: 

https://gcc.gnu.org/onlinedocs/gcc/Optimize-Options.html

 

Jiri

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,412 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

 

s32ds uses gcc compiler - the optimization level description you can find here: 

https://gcc.gnu.org/onlinedocs/gcc/Optimize-Options.html

 

Jiri

0 项奖励
回复
2,391 次查看
StarMao159376
Contributor II

Thanks.

0 项奖励
回复