S32 design studio for S32 platform 3.4 installation failed (Windows 11)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32 design studio for S32 platform 3.4 installation failed (Windows 11)

跳至解决方案
3,148 次查看
CoderSun
Contributor I

Hello everyone,

I had the following problem while installing S32 Design Studio for Platform 3.4.

The screenshot below:

CoderSun_0-1642399454990.png

The log file below:

Install Uninstaller: S32 Design Studio for S32 Platform 3.4(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

Uninstall Folder: D:\NXP\S32DS.3.4\jre
Status: SUCCESSFUL

Uninstall Folder: C:\Users\Xun Sun\AppData\Local\Temp\291549.tmp\FNPLicensingService
Status: WARNING
Additional Notes: WARNING - The path does not exist

Uninstall Folder: C:\Users\Xun Sun\AppData\Local\Temp\291549.tmp\cll\x64
Status: WARNING
Additional Notes: WARNING - The path does not exist

Uninstall Folder: C:\Users\Xun Sun\AppData\Local\Temp\291549.tmp\cll\i86
Status: WARNING
Additional Notes: WARNING - The path does not exist

Uninstall Folder: C:\Users\Xun Sun\AppData\Local\Temp\291549.tmp\cll
Status: WARNING
Additional Notes: WARNING - The path does not exist

0 项奖励
回复
1 解答
3,058 次查看
mikedoidge
NXP Employee
NXP Employee

Hello Cylus,

The S32 Design Studio does not yet support Windows 11. No testing has been done for this. It is unknown what issues might arise from this. I suggest you look for a compatibility mode option on the installer file, perhaps that will resolve this error?

Best Regards,

Mike

在原帖中查看解决方案

1 回复
3,059 次查看
mikedoidge
NXP Employee
NXP Employee

Hello Cylus,

The S32 Design Studio does not yet support Windows 11. No testing has been done for this. It is unknown what issues might arise from this. I suggest you look for a compatibility mode option on the installer file, perhaps that will resolve this error?

Best Regards,

Mike