S32 design studio example project[hello] issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 design studio example project[hello] issue

2,697件の閲覧回数
sooyeonkang
Contributor I

I imported a project that was based on the gpio example(project name = hello) for the S32k144 board. And the project comple is OK.

Running result is correct. But after power off and on, it doesn't run firmware.

I expect that the project always run if power is on.

 

However a project I created is OK.

 

One project I imported and Another project I created use equal source code.

 

Why running result differ from two projects?

ラベル(1)
タグ(3)
2 返答(返信)

2,341件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

Can you possibly attach the project you imported?

I'll check it.

Thanks!

Stan

2,341件の閲覧回数
sykang
Contributor I

Hello, Stan.

Sorry for my late reply.

This is the project link.

Link : GPIO.tar.gz - Google Drive 

Please check this project.

Thanks.

Sooyeon

0 件の賞賛
返信