S32 design studio example project[hello] issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 design studio example project[hello] issue

2,677 Views
sooyeonkang
Contributor I

I imported a project that was based on the gpio example(project name = hello) for the S32k144 board. And the project comple is OK.

Running result is correct. But after power off and on, it doesn't run firmware.

I expect that the project always run if power is on.

 

However a project I created is OK.

 

One project I imported and Another project I created use equal source code.

 

Why running result differ from two projects?

Labels (1)
2 Replies

2,321 Views
stanish
NXP Employee
NXP Employee

Hi,

Can you possibly attach the project you imported?

I'll check it.

Thanks!

Stan

2,321 Views
sykang
Contributor I

Hello, Stan.

Sorry for my late reply.

This is the project link.

Link : GPIO.tar.gz - Google Drive 

Please check this project.

Thanks.

Sooyeon

0 Kudos
Reply