S32 can not be installed, prompting you do not have enough Windows Permissions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 can not be installed, prompting you do not have enough Windows Permissions

Jump to solution
12,099 Views
xiao_fu
Contributor II

The two win10 computers can't follow, what compatibility mode, administrator rights have tried many times

__________________________________________________________________________

Wed Apr 29 03:23:19 CST 2020

Free Memory: 32849 kB
Total Memory: 48084 kB

java.class.path:
Z:\TEMP\I1588144798\InstallerData\IAClasses.zip
Z:\TEMP\I1588144798\InstallerData\Execute.zip
Z:\TEMP\I1588144798\Windows\InstallerData\Execute.zip
Z:\TEMP\I1588144798\InstallerData\Resource1.zip
Z:\TEMP\I1588144798\Windows\InstallerData\Resource1.zip
Z:\TEMP\I1588144798\InstallerData
Z:\TEMP\I1588144798\Windows\InstallerData

ZGUtil.CLASS_PATH:
Z:\TEMP\I1588144798\InstallerData\IAClasses.zip
Z:\TEMP\I1588144798\InstallerData\Execute.zip
Z:\TEMP\I1588144798\InstallerData

sun.boot.class.path:
Z:\TEMP\I1588144798\Windows\resource\jre\lib\resources.jar
Z:\TEMP\I1588144798\Windows\resource\jre\lib\rt.jar
Z:\TEMP\I1588144798\Windows\resource\jre\lib\sunrsasign.jar
Z:\TEMP\I1588144798\Windows\resource\jre\lib\jsse.jar
Z:\TEMP\I1588144798\Windows\resource\jre\lib\jce.jar
Z:\TEMP\I1588144798\Windows\resource\jre\lib\charsets.jar
Z:\TEMP\I1588144798\Windows\resource\jre\lib\jfr.jar
Z:\TEMP\I1588144798\Windows\resource\jre\classes

java.ext.dirs:
Z:\TEMP\I1588144798\Windows\resource\jre\lib\ext
C:\Windows\Sun\Java\lib\ext

java.version == 1.8.0_202 (Java 1)
java.vm.name == Java HotSpot(TM) Client VM
java.vm.vendor == Oracle Corporation
java.vm.version == 25.202-b08
java.vm.specification.name == Java Virtual Machine Specification
java.vm.specification.vendor == Oracle Corporation
java.vm.specification.version == 1.8
java.specification.name == Java Platform API Specification
java.specification.vendor == Oracle Corporation
java.specification.version == 1.8
java.vendor == Oracle Corporation
java.vendor.url == http://java.oracle.com/
java.class.version == 52.0
java.library.path == Z:\TEMP\I1588144798\Windows\resource\jre\bin;C:\Windows\Sun\Java\bin;C:\Windows\system32;C:\Windows;C:\Program Files (x86)\Common Files\Oracle\Java\javapath;C:\Program Files\Typhoon HIL Control Center 2020.1\bin\;C:\Python37\Scripts\;C:\Python37\;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Windows\System32\OpenSSH\;C:\Program Files (x86)\NVIDIA Corporation\PhysX\Common;C:\Program Files\NVIDIA Corporation\NVIDIA NvDLISR;C:\MATLAB\R2018b\runtime\win64;C:\MATLAB\R2018b\bin;C:\MATLAB\R2015a\bin;C:\Program Files\Microsoft Windows Performance Toolkit\;D:\PythonProject\venv\Lib\site-packages\pyqt5_tools\Qt\bin;C:\Program Files (x86)\National Instruments\Shared\LabVIEW CLI;C:\Users\fuxia\AppData\Local\Microsoft\WindowsApps;C:\Program Files\JetBrains\CLion 2019.3.2\bin;C:\Program Files\JetBrains\PyCharm 2019.3.1\bin;.
java.compiler == null
java.home == Z:\TEMP\I1588144798\Windows\resource\jre
java.io.tmpdir == Z:\TEMP\
os.name == Microsoft Windows 10 家庭中文版
os.arch == x86
os.version == 10.0.18363
path.separator == ;
file.separator == \
file.encoding == GBK
user.name == fuxia
user.home == C:\Users\fuxia
user.dir == Z:\TEMP\I1588144798\Windows
user.language == en
user.region == null
__________________________________________________________________________

Installed Feature(s) S32DSF, FreeM of S32 Design Studio for Power Architecture Version 2.1

Install Begin: APRIL 29, 2020 3:21:17 PM CST
Install End: APRIL 29, 2020 3:22:18 PM CST

Installed by InstallAnywhere 18.0 Professional Build 5608


User Interactions
-----------------


#Choose additional feature(s)
#----------------------------
CHOSEN_FEATURE_LIST=S32DSF,FreeM
CHOSEN_INSTALL_FEATURE_LIST=S32DSF,FreeM
CHOSEN_INSTALL_SET=Add

#Choose Install Location
#-----------------------
USER_INSTALL_DIR=C:\\NXP\\S32DS_Power_v2.1

#Choose Shortcut Folder
#----------------------
USER_SHORTCUTS=C:\\Users\\fuxia\\OneDrive\\桌面

#Install
#-------
-fileOverwrite_C\:\\NXP\\S32DS_Power_v2.1\\_S32\ Design\ Studio\ for\ Power\ Architecture\ Version\ 2.1_installation\\resource\\iawin32.dll=Yes
-fileOverwrite_C\:\\NXP\\S32DS_Power_v2.1\\_S32\ Design\ Studio\ for\ Power\ Architecture\ Version\ 2.1_installation\\resource\\win64_32_x64.exe=Yes
-fileOverwrite_C\:\\NXP\\S32DS_Power_v2.1\\_S32\ Design\ Studio\ for\ Power\ Architecture\ Version\ 2.1_installation\\resource\\remove.exe=Yes
-fileOverwrite_C\:\\NXP\\S32DS_Power_v2.1\\_S32\ Design\ Studio\ for\ Power\ Architecture\ Version\ 2.1_installation\\resource\\invoker.exe=Yes

Summary
-------

Installation: Unsuccessful.

17 Successes
0 Warnings
1 NonFatalErrors
1 FatalErrors

Action Notes:

None

Install Log Detail:

Check Disk Space: C:\NXP\S32DS__v2.1
Status: SUCCESSFUL
Additional Notes: NOTE - Required Disk Space:7,110,783,442 Bytes Free Disk Space:326,346,653,696 Bytes

Check Disk Space: C:\NXP\S32DS_Power_v2.1
Status: SUCCESSFUL
Additional Notes: NOTE - Required Disk Space:7,153,215,311 Bytes Free Disk Space:326,346,653,696 Bytes

Install Directory: C:\NXP\S32DS_Power_v2.1\jre
Status: SUCCESSFUL

Install JRE: C:\NXP\S32DS_Power_v2.1\jre
Status: SUCCESSFUL

Install Directory: Z:\TEMP\735982.tmp\
Status: SUCCESSFUL
Additional Notes: NOTE - Directory already existed

Execute Command: NET SESSION
Status: SUCCESSFUL

Execute Command: ping 1.1.1.1 -n 11
Status: SUCCESSFUL

Install Uninstaller: S32 Design Studio for Power Architecture Version 2.1(Install All Uninstaller Components)
Status: SUCCESSFUL

Install Directory: C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\resource\
Status: SUCCESSFUL

Install File: C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\resource\iawin32.dll
Status: SUCCESSFUL

Install File: C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\resource\win64_32_x64.exe
Status: SUCCESSFUL

Install File: C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\resource\remove.exe
Status: SUCCESSFUL

Install File: C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\resource\invoker.exe
Status: SUCCESSFUL

Install Uninstaller: S32 Design Studio for Power Architecture Version 2.1(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

Uninstall Folder: C:\NXP\S32DS_Power_v2.1\jre
Status: SUCCESSFUL

Remove Registry Entry: 5 HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\Uninstall\null
Status: SUCCESSFUL

Error occurred while installing the following Action, hence rolling back the installation....!


Action Name: Trigger Rollback Action
Action Description: Trigger Rollback Action


Error Details as below:


This action rolls back the Installation.
====================STDERR ENTRIES==================

__________________________________________________________________________

InstallAnywhere 2017
Version: 18.0
__________________________________________________________________________

Wed Apr 29 03:21:15 CST 2020

Free Memory: 10691 kB
Total Memory: 15872 kB

No Arguments

java.class.path:
Z:\TEMP\I1588144798\InstallerData\IAClasses.zip
Z:\TEMP\I1588144798\InstallerData\Execute.zip
Z:\TEMP\I1588144798\Windows\InstallerData\Execute.zip
Z:\TEMP\I1588144798\InstallerData\Resource1.zip
Z:\TEMP\I1588144798\Windows\InstallerData\Resource1.zip
Z:\TEMP\I1588144798\InstallerData
Z:\TEMP\I1588144798\Windows\InstallerData

ZGUtil.CLASS_PATH:
Z:\TEMP\I1588144798\InstallerData\IAClasses.zip
Z:\TEMP\I1588144798\InstallerData\Execute.zip
Z:\TEMP\I1588144798\InstallerData

sun.boot.class.path:
Z:\TEMP\I1588144798\Windows\resource\jre\lib\resources.jar
Z:\TEMP\I1588144798\Windows\resource\jre\lib\rt.jar
Z:\TEMP\I1588144798\Windows\resource\jre\lib\sunrsasign.jar
Z:\TEMP\I1588144798\Windows\resource\jre\lib\jsse.jar
Z:\TEMP\I1588144798\Windows\resource\jre\lib\jce.jar
Z:\TEMP\I1588144798\Windows\resource\jre\lib\charsets.jar
Z:\TEMP\I1588144798\Windows\resource\jre\lib\jfr.jar
Z:\TEMP\I1588144798\Windows\resource\jre\classes

java.ext.dirs:
Z:\TEMP\I1588144798\Windows\resource\jre\lib\ext
C:\Windows\Sun\Java\lib\ext

java.version == 1.8.0_202 (Java 1)
java.vm.name == Java HotSpot(TM) Client VM
java.vm.vendor == Oracle Corporation
java.vm.version == 25.202-b08
java.vm.specification.name == Java Virtual Machine Specification
java.vm.specification.vendor == Oracle Corporation
java.vm.specification.version == 1.8
java.specification.name == Java Platform API Specification
java.specification.vendor == Oracle Corporation
java.specification.version == 1.8
java.vendor == Oracle Corporation
java.vendor.url == http://java.oracle.com/
java.class.version == 52.0
java.library.path == Z:\TEMP\I1588144798\Windows\resource\jre\bin;C:\Windows\Sun\Java\bin;C:\Windows\system32;C:\Windows;C:\Program Files (x86)\Common Files\Oracle\Java\javapath;C:\Program Files\Typhoon HIL Control Center 2020.1\bin\;C:\Python37\Scripts\;C:\Python37\;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Windows\System32\OpenSSH\;C:\Program Files (x86)\NVIDIA Corporation\PhysX\Common;C:\Program Files\NVIDIA Corporation\NVIDIA NvDLISR;C:\MATLAB\R2018b\runtime\win64;C:\MATLAB\R2018b\bin;C:\MATLAB\R2015a\bin;C:\Program Files\Microsoft Windows Performance Toolkit\;D:\PythonProject\venv\Lib\site-packages\pyqt5_tools\Qt\bin;C:\Program Files (x86)\National Instruments\Shared\LabVIEW CLI;C:\Users\fuxia\AppData\Local\Microsoft\WindowsApps;C:\Program Files\JetBrains\CLion 2019.3.2\bin;C:\Program Files\JetBrains\PyCharm 2019.3.1\bin;.
java.compiler == null
java.home == Z:\TEMP\I1588144798\Windows\resource\jre
java.io.tmpdir == Z:\TEMP\
os.name == Microsoft Windows 10 家庭中文版
os.arch == x86
os.version == 10.0.18363
path.separator == ;
file.separator == \
file.encoding == GBK
user.name == fuxia
user.home == C:\Users\fuxia
user.dir == Z:\TEMP\I1588144798\Windows
user.language == zh
user.region == null
__________________________________________________________________________

Loading externalized properties


RepositoryManager: Trying fallback repository location...
#
# INSTALLING VM: C:\NXP\S32DS_Power_v2.1\jre
#
System's temporary directory = Z:\TEMP
XMLScriptWriter: No Installation Objects were skipped
8. final log file name=C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\Logs\S32_Design_Studio_for_Power_Architecture_Version_2.1_Install_04_29_2020_15_23_19.log

====================STDOUT ENTRIES==================

C:\NXP\S32DS_Power_v2.1\jre
C:\NXP\S32DS_Power_v2.1\jre\bin
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-console-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-datetime-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-debug-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-errorhandling-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-file-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-file-l1-2-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-file-l2-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-handle-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-heap-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-interlocked-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-libraryloader-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-localization-l1-2-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-memory-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-namedpipe-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-processenvironment-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-processthreads-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-processthreads-l1-1-1.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-profile-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-rtlsupport-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-string-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-synch-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-synch-l1-2-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-sysinfo-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-timezone-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-core-util-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-crt-conio-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-crt-convert-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-crt-environment-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-crt-filesystem-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-crt-heap-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-crt-locale-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-crt-math-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-crt-multibyte-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-crt-private-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-crt-process-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-crt-runtime-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-crt-stdio-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-crt-string-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-crt-time-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\api-ms-win-crt-utility-l1-1-0.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\awt.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\bci.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\client
C:\NXP\S32DS_Power_v2.1\jre\bin\client\jvm.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\client\Xusage.txt
C:\NXP\S32DS_Power_v2.1\jre\bin\concrt140.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\dcpr.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\decora_sse.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\deploy.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\dtplugin
C:\NXP\S32DS_Power_v2.1\jre\bin\dtplugin\deployJava1.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\dtplugin\npdeployJava1.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\dt_shmem.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\dt_socket.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\eula.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\fontmanager.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\fxplugins.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\glass.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\glib-lite.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\gstreamer-lite.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\hprof.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\instrument.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\j2pcsc.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\j2pkcs11.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\jaas_nt.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\jabswitch.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\java-rmi.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\java.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\java.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\JavaAccessBridge-32.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\JavaAccessBridge.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\javacpl.cpl
C:\NXP\S32DS_Power_v2.1\jre\bin\javacpl.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\javafx_font.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\javafx_font_t2k.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\javafx_iio.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\javaw.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\javaws.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\java_crw_demo.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\jawt.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\JAWTAccessBridge-32.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\JAWTAccessBridge.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\jdwp.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\jfr.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\jfxmedia.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\jfxwebkit.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\jjs.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\jli.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\jp2iexp.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\jp2launcher.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\jp2native.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\jp2ssv.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\jpeg.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\jsdt.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\jsound.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\jsoundds.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\keytool.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\kinit.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\klist.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\ktab.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\lcms.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\management.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\mlib_image.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\msvcp140.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\msvcr100.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\net.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\nio.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\npt.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\orbd.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\pack200.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\plugin2
C:\NXP\S32DS_Power_v2.1\jre\bin\plugin2\msvcr100.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\plugin2\npjp2.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\policytool.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\prism_common.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\prism_d3d.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\prism_sw.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\resource.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\rmid.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\rmiregistry.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\servertool.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\splashscreen.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\ssv.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\ssvagent.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\sunec.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\sunmscapi.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\t2k.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\tnameserv.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\ucrtbase.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\unpack.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\unpack200.exe
C:\NXP\S32DS_Power_v2.1\jre\bin\vcruntime140.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\verify.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\w2k_lsa_auth.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\WindowsAccessBridge-32.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\WindowsAccessBridge.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\wsdetect.dll
C:\NXP\S32DS_Power_v2.1\jre\bin\zip.dll
C:\NXP\S32DS_Power_v2.1\jre\COPYRIGHT
C:\NXP\S32DS_Power_v2.1\jre\lib
C:\NXP\S32DS_Power_v2.1\jre\lib\accessibility.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\calendars.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\charsets.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\classlist
C:\NXP\S32DS_Power_v2.1\jre\lib\cmm
C:\NXP\S32DS_Power_v2.1\jre\lib\cmm\CIEXYZ.pf
C:\NXP\S32DS_Power_v2.1\jre\lib\cmm\GRAY.pf
C:\NXP\S32DS_Power_v2.1\jre\lib\cmm\LINEAR_RGB.pf
C:\NXP\S32DS_Power_v2.1\jre\lib\cmm\PYCC.pf
C:\NXP\S32DS_Power_v2.1\jre\lib\cmm\sRGB.pf
C:\NXP\S32DS_Power_v2.1\jre\lib\content-types.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\currency.data
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\ffjcext.zip
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\messages.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\messages_de.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\messages_es.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\messages_fr.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\messages_it.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\messages_ja.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\messages_ko.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\messages_pt_BR.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\messages_sv.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\messages_zh_CN.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\messages_zh_HK.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\messages_zh_TW.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\splash.gif
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\splash@2x.gif
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\splash_11-lic.gif
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy\splash_11@2x-lic.gif
C:\NXP\S32DS_Power_v2.1\jre\lib\deploy.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\ext
C:\NXP\S32DS_Power_v2.1\jre\lib\ext\access-bridge-32.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\ext\access-bridge.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\ext\cldrdata.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\ext\dnsns.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\ext\jaccess.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\ext\jfxrt.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\ext\localedata.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\ext\meta-index
C:\NXP\S32DS_Power_v2.1\jre\lib\ext\nashorn.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\ext\sunec.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\ext\sunjce_provider.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\ext\sunmscapi.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\ext\sunpkcs11.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\ext\zipfs.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\flavormap.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\fontconfig.bfc
C:\NXP\S32DS_Power_v2.1\jre\lib\fontconfig.properties.src
C:\NXP\S32DS_Power_v2.1\jre\lib\fonts
C:\NXP\S32DS_Power_v2.1\jre\lib\fonts\LucidaBrightDemiBold.ttf
C:\NXP\S32DS_Power_v2.1\jre\lib\fonts\LucidaBrightDemiItalic.ttf
C:\NXP\S32DS_Power_v2.1\jre\lib\fonts\LucidaBrightItalic.ttf
C:\NXP\S32DS_Power_v2.1\jre\lib\fonts\LucidaBrightRegular.ttf
C:\NXP\S32DS_Power_v2.1\jre\lib\fonts\LucidaSansDemiBold.ttf
C:\NXP\S32DS_Power_v2.1\jre\lib\fonts\LucidaSansRegular.ttf
C:\NXP\S32DS_Power_v2.1\jre\lib\fonts\LucidaTypewriterBold.ttf
C:\NXP\S32DS_Power_v2.1\jre\lib\fonts\LucidaTypewriterRegular.ttf
C:\NXP\S32DS_Power_v2.1\jre\lib\hijrah-config-umalqura.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\i386
C:\NXP\S32DS_Power_v2.1\jre\lib\i386\jvm.cfg
C:\NXP\S32DS_Power_v2.1\jre\lib\images
C:\NXP\S32DS_Power_v2.1\jre\lib\images\cursors
C:\NXP\S32DS_Power_v2.1\jre\lib\images\cursors\cursors.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\images\cursors\invalid32x32.gif
C:\NXP\S32DS_Power_v2.1\jre\lib\images\cursors\win32_CopyDrop32x32.gif
C:\NXP\S32DS_Power_v2.1\jre\lib\images\cursors\win32_CopyNoDrop32x32.gif
C:\NXP\S32DS_Power_v2.1\jre\lib\images\cursors\win32_LinkDrop32x32.gif
C:\NXP\S32DS_Power_v2.1\jre\lib\images\cursors\win32_LinkNoDrop32x32.gif
C:\NXP\S32DS_Power_v2.1\jre\lib\images\cursors\win32_MoveDrop32x32.gif
C:\NXP\S32DS_Power_v2.1\jre\lib\images\cursors\win32_MoveNoDrop32x32.gif
C:\NXP\S32DS_Power_v2.1\jre\lib\javafx.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\javaws.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\jce.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\jfr
C:\NXP\S32DS_Power_v2.1\jre\lib\jfr\default.jfc
C:\NXP\S32DS_Power_v2.1\jre\lib\jfr\profile.jfc
C:\NXP\S32DS_Power_v2.1\jre\lib\jfr.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\jfxswt.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\jsse.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\jvm.hprof.txt
C:\NXP\S32DS_Power_v2.1\jre\lib\logging.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\management
C:\NXP\S32DS_Power_v2.1\jre\lib\management\jmxremote.access
C:\NXP\S32DS_Power_v2.1\jre\lib\management\jmxremote.password.template
C:\NXP\S32DS_Power_v2.1\jre\lib\management\management.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\management\snmp.acl.template
C:\NXP\S32DS_Power_v2.1\jre\lib\management-agent.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\meta-index
C:\NXP\S32DS_Power_v2.1\jre\lib\net.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\plugin.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\psfont.properties.ja
C:\NXP\S32DS_Power_v2.1\jre\lib\psfontj2d.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\resources.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\rt.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\security
C:\NXP\S32DS_Power_v2.1\jre\lib\security\blacklist
C:\NXP\S32DS_Power_v2.1\jre\lib\security\blacklisted.certs
C:\NXP\S32DS_Power_v2.1\jre\lib\security\cacerts
C:\NXP\S32DS_Power_v2.1\jre\lib\security\java.policy
C:\NXP\S32DS_Power_v2.1\jre\lib\security\java.security
C:\NXP\S32DS_Power_v2.1\jre\lib\security\javaws.policy
C:\NXP\S32DS_Power_v2.1\jre\lib\security\policy
C:\NXP\S32DS_Power_v2.1\jre\lib\security\policy\limited
C:\NXP\S32DS_Power_v2.1\jre\lib\security\policy\limited\local_policy.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\security\policy\limited\US_export_policy.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\security\policy\unlimited
C:\NXP\S32DS_Power_v2.1\jre\lib\security\policy\unlimited\local_policy.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\security\policy\unlimited\US_export_policy.jar
C:\NXP\S32DS_Power_v2.1\jre\lib\security\trusted.libraries
C:\NXP\S32DS_Power_v2.1\jre\lib\sound.properties
C:\NXP\S32DS_Power_v2.1\jre\lib\tzdb.dat
C:\NXP\S32DS_Power_v2.1\jre\lib\tzmappings
C:\NXP\S32DS_Power_v2.1\jre\LICENSE
C:\NXP\S32DS_Power_v2.1\jre\README.txt
C:\NXP\S32DS_Power_v2.1\jre\release
C:\NXP\S32DS_Power_v2.1\jre\THIRDPARTYLICENSEREADME-JAVAFX.txt
C:\NXP\S32DS_Power_v2.1\jre\THIRDPARTYLICENSEREADME.txt
C:\NXP\S32DS_Power_v2.1\jre\Welcome.html
C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation
C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\.com.zerog.registry.xml
C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\InstallScript.iap_xml
C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\Logs
C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\Logs\S32_Design_Studio_for_Power_Architecture_Version_2.1_Install_04_29_2020_14_57_06.log
C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\Logs\S32_Design_Studio_for_Power_Architecture_Version_2.1_Install_04_29_2020_15_19_44.log
C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\resource
C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\resource\iawin32.dll
C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\resource\invoker.exe
C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\resource\remove.exe
C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\resource\win64_32_x64.exe
C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\uninstaller.jar

微信图片_20200429153248.png

0 Kudos
Reply
1 Solution
11,879 Views
xiao_fu
Contributor II

Hi Jiri,     I've solved the problem by starting the 'server' service on Windows. Thanks!

 

 

 

 

View solution in original post

0 Kudos
Reply
9 Replies
9,384 Views
Sandy90
Contributor I

The issue of "You don't have enough windows permissions" while installing S32 Design studio 3.5 is still coming even after running the Windows "Server" service. Can anyone help to resolve the issue? Thanks in advance.

0 Kudos
Reply
9,304 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, Santosh, 

There was some issue last week with server was not working, please can you check again, reinstalling if it works. 

Please make sure that you have administrator rights while installation. 

 

Also check with your company's IT team, if firewall blocking or any other issue. 

 

Please follow this guide for activation: 

 https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Activate-S32-Design-Studio/ta-p/...

 

Please follow the S32DS guide while installing S32DS: https://www.nxp.com/webapp/Download?colCode=S32DSIG

 

If you are still having issue. Please update us. 

 

Thank you. Best regards. 

- Mehul Patel 

Tags (2)
0 Kudos
Reply
9,862 Views
Elvis
Contributor I

你好,我也遇到了,请问最后怎么解决的?

0 Kudos
Reply
11,868 Views
414563072
Contributor I

Hi xiaofu:

            Did you solve your problem? I have the same problem, please share the experience。  Email:414563072@qq.com

0 Kudos
Reply
11,868 Views
mso
NXP Employee
NXP Employee

Hello Zhihaiyang,

Please read this thread through; the issue may be caused by your specific Windows configuration. In some cases users are not Administrators on their PC. But Xiaofu had Windows service "Server" not running (that service works with network subsystem and the Installer in turn uses it just to check if user permissions can be elevated for proper install).

Thanks,
Mikhail

0 Kudos
Reply
11,868 Views
alexeyshuginin
NXP Employee
NXP Employee

Good evening,

I’d suggest to check NET SESSION command output and exit code.

Installer use it to check if the user is a member of Administrators group.

Also please try to create a file at the following directories:

USER_INSTALL_DIR=C:\\NXP\\S32DS_Power_v2.1

USER_SHORTCUTS=C:\\Users\\fuxia\\OneDrive\\桌面

user.dir == Z:\TEMP\I1588144798\Windows

Thank you,

Alexey.

0 Kudos
Reply
11,868 Views
xiao_fu
Contributor II

 Hi Alexey,

     I've solved the problem by starting the 'server' service on Windows. Thanks!

 

 

0 Kudos
Reply
11,868 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks that for some reason installer can't write *.jar files into C:\NXP\S32DS_Power_v2.1\_S32 Design Studio for Power Architecture Version 2.1_installation\  folder. XML file is okay. I'll try figure out it  with IDE team.  

Jiri

 

0 Kudos
Reply
11,880 Views
xiao_fu
Contributor II

Hi Jiri,     I've solved the problem by starting the 'server' service on Windows. Thanks!

 

 

 

 

0 Kudos
Reply