S32 Flash Tool failure to establish communication with device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32 Flash Tool failure to establish communication with device

跳至解决方案
2,190 次查看
Alex_mjl
Contributor II

Hi NXP,

  I am using the S32G-VNP-RDB2 evaluation board (S32G274A).

  According to "S32G-VNP-RDB2" I configured the DIP Switches following the "3.1 Default Switch Setting" setting, but also change for the "3.6 Switch Setting for Serial Boot".

Alex_mjl_0-1698141607029.pngAlex_mjl_1-1698141619396.png

  Settings for the UART COM which is connected to UART0.

Alex_mjl_0-1698141910791.png

 

  Then I use the flash tool to burn binary files into EMMC:

Alex_mjl_3-1698141791911.png

 It's always failure to establish communication with target device.

 

0 项奖励
回复
1 解答
2,166 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We understand that SW3 is in the default position, is this correct? If so, you are selecting the SD instead of the EMMC. You require to change the SW3 as shown below:

DanielAguirre_1-1698172957732.png

Just SW3, since serial boot is as you shown on the second image.

After this, you should be able to load the algorithm and detect the EMMC available under the RDB2.

Please, let us know.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,167 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We understand that SW3 is in the default position, is this correct? If so, you are selecting the SD instead of the EMMC. You require to change the SW3 as shown below:

DanielAguirre_1-1698172957732.png

Just SW3, since serial boot is as you shown on the second image.

After this, you should be able to load the algorithm and detect the EMMC available under the RDB2.

Please, let us know.

0 项奖励
回复
2,161 次查看
Alex_mjl
Contributor II

Thanks, the problem is that sw3 three is not configured correctly.

0 项奖励
回复