S32 Flash Tool failure to establish communication with device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Flash Tool failure to establish communication with device

Jump to solution
2,154 Views
Alex_mjl
Contributor II

Hi NXP,

  I am using the S32G-VNP-RDB2 evaluation board (S32G274A).

  According to "S32G-VNP-RDB2" I configured the DIP Switches following the "3.1 Default Switch Setting" setting, but also change for the "3.6 Switch Setting for Serial Boot".

Alex_mjl_0-1698141607029.pngAlex_mjl_1-1698141619396.png

  Settings for the UART COM which is connected to UART0.

Alex_mjl_0-1698141910791.png

 

  Then I use the flash tool to burn binary files into EMMC:

Alex_mjl_3-1698141791911.png

 It's always failure to establish communication with target device.

 

0 Kudos
Reply
1 Solution
2,130 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We understand that SW3 is in the default position, is this correct? If so, you are selecting the SD instead of the EMMC. You require to change the SW3 as shown below:

DanielAguirre_1-1698172957732.png

Just SW3, since serial boot is as you shown on the second image.

After this, you should be able to load the algorithm and detect the EMMC available under the RDB2.

Please, let us know.

View solution in original post

0 Kudos
Reply
2 Replies
2,131 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We understand that SW3 is in the default position, is this correct? If so, you are selecting the SD instead of the EMMC. You require to change the SW3 as shown below:

DanielAguirre_1-1698172957732.png

Just SW3, since serial boot is as you shown on the second image.

After this, you should be able to load the algorithm and detect the EMMC available under the RDB2.

Please, let us know.

0 Kudos
Reply
2,125 Views
Alex_mjl
Contributor II

Thanks, the problem is that sw3 three is not configured correctly.

0 Kudos
Reply