S32 Design studio for power architecture 2.1 installation failure on Windows

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32 Design studio for power architecture 2.1 installation failure on Windows

跳至解决方案
3,464 次查看
sumityadav
Contributor II

Confirmed that the activation code is good, was able to succesfully install on other computers but unable to on this machine.

Hello!

Installation log shows the following error:

Install Uninstaller: S32 Design Studio for Power Architecture Version 2.1(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

What does this mean? I am running the installer as admin.

Full log is attached.

Thanks!

0 项奖励
回复
1 解答
3,437 次查看
mikedoidge
NXP Employee
NXP Employee

Hello,

It is possible some file became corrupted during the installation process. It is also possible that the trusted storage was corrupted. Please try removing the trusted storage by the following and then retry the installation.

delete C:\ProgramData\FLEXNet.

 

Best Regards,

Mike

在原帖中查看解决方案

3 回复数
3,434 次查看
sumityadav
Contributor II

Deleting C:\ProgramData\FLEXNet worked!

thanks so much Mike!

0 项奖励
回复
3,438 次查看
mikedoidge
NXP Employee
NXP Employee

Hello,

It is possible some file became corrupted during the installation process. It is also possible that the trusted storage was corrupted. Please try removing the trusted storage by the following and then retry the installation.

delete C:\ProgramData\FLEXNet.

 

Best Regards,

Mike

2,955 次查看
Hwanmin
Contributor II

thank you very much
thank you very much......
very very really
Thank you......

0 项奖励
回复