S32 Design studio for power architecture 2.1 installation failure on Windows

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design studio for power architecture 2.1 installation failure on Windows

ソリューションへジャンプ
2,455件の閲覧回数
sumityadav
Contributor II

Confirmed that the activation code is good, was able to succesfully install on other computers but unable to on this machine.

Hello!

Installation log shows the following error:

Install Uninstaller: S32 Design Studio for Power Architecture Version 2.1(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

What does this mean? I am running the installer as admin.

Full log is attached.

Thanks!

0 件の賞賛
返信
1 解決策
2,428件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello,

It is possible some file became corrupted during the installation process. It is also possible that the trusted storage was corrupted. Please try removing the trusted storage by the following and then retry the installation.

delete C:\ProgramData\FLEXNet.

 

Best Regards,

Mike

元の投稿で解決策を見る

3 返答(返信)
2,425件の閲覧回数
sumityadav
Contributor II

Deleting C:\ProgramData\FLEXNet worked!

thanks so much Mike!

0 件の賞賛
返信
2,429件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello,

It is possible some file became corrupted during the installation process. It is also possible that the trusted storage was corrupted. Please try removing the trusted storage by the following and then retry the installation.

delete C:\ProgramData\FLEXNet.

 

Best Regards,

Mike

1,946件の閲覧回数
Hwanmin
Contributor II

thank you very much
thank you very much......
very very really
Thank you......

0 件の賞賛
返信