S32 Design studio for power architecture 2.1 installation failure on Windows

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design studio for power architecture 2.1 installation failure on Windows

Jump to solution
3,412 Views
sumityadav
Contributor II

Confirmed that the activation code is good, was able to succesfully install on other computers but unable to on this machine.

Hello!

Installation log shows the following error:

Install Uninstaller: S32 Design Studio for Power Architecture Version 2.1(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

What does this mean? I am running the installer as admin.

Full log is attached.

Thanks!

0 Kudos
Reply
1 Solution
3,385 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

It is possible some file became corrupted during the installation process. It is also possible that the trusted storage was corrupted. Please try removing the trusted storage by the following and then retry the installation.

delete C:\ProgramData\FLEXNet.

 

Best Regards,

Mike

View solution in original post

3 Replies
3,382 Views
sumityadav
Contributor II

Deleting C:\ProgramData\FLEXNet worked!

thanks so much Mike!

0 Kudos
Reply
3,386 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

It is possible some file became corrupted during the installation process. It is also possible that the trusted storage was corrupted. Please try removing the trusted storage by the following and then retry the installation.

delete C:\ProgramData\FLEXNet.

 

Best Regards,

Mike

2,903 Views
Hwanmin
Contributor II

thank you very much
thank you very much......
very very really
Thank you......

0 Kudos
Reply