Hi @Bernez,
When importing your project, S32DS throws me many errors in configuration for the SDK, as such:
Julin_AragnM_0-1708107685007.png
As well as some path problems;
Julin_AragnM_1-1708107722128.png
This seems to be a problem with the project configuration for the KSDK specific path:
Julin_AragnM_2-1708107848712.png
Could you try installing S32 Design Studio for Arm v2.0 - Update 3, which includes S32K14x_EAR_0.8.6? This seems to fix the SDK path value issue:
Julin_AragnM_3-1708107902423.png
Once this update is installed, please try importing the project I have shared into the workspace, the same way you already explained in the original post: Import > Existing Project Into Workspace > Select archive file > Finish
Once imported, move the Baudrate configuration first, generate Processor Expert Code which should prompt a "Track Changes" window:
Julin_AragnM_4-1708108182778.png
After accepting and waiting for the code to be generated, the project should be able to be built:
Julin_AragnM_5-1708108220632.png
If this is still not the case, I would suggest reinstalling S32DS, and only adding update 2 and 3, and testing these steps again, as your workspace or installation may have been broken.
I have also added the build log, and some project properties for the C Build, as you error seems to be related to the makefile, so you can compare:
Julin_AragnM_10-1708108446794.png
Julin_AragnM_9-1708108435715.png
Best regards,
Julián.