S32 Design Studio for Power Architecture, Version 2017.R1 update patch failed.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for Power Architecture, Version 2017.R1 update patch failed.

1,973件の閲覧回数
Zhangxq
Contributor I

when i update the software from the website.it will be show below trouble,CAN YOU HELP ME?An error occurred while collecting items to be installed
session context was:(profile=SDKProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=null --> [R]com.nxp.s32ds.cross.sdk.S32PA_1.8.0.brc_root 1.0.0.201811261458, action=).
The required Touchpoint: com.freescale.updater.touchpoint 1.0.0 touchpoint for the collect action is not included in the installation manager configuration.
The required Touchpoint: com.freescale.updater.touchpoint 1.0.0 touchpoint for the collect action is not included in the installation manager configuration.

 

Thanks

0 件の賞賛
返信
1 返信

1,952件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @Zhangxq,

I am unable to reproduce the issue. It is quite unusual.

Have you tried to reboot the machine and relaunch S32 Design Studio?

It is possible that some file had become corrupt. Try uninstalling and then reinstalling S32 Design Studio.

Best Regards,

Mike

0 件の賞賛
返信