S32 Design Studio for ARM (Linux)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Design Studio for ARM (Linux)

22,397 次查看
amitwarbhe
Contributor I

Even with admin privilege not able to install this binary on ubuntu - 22.04 with activation code - 1992-D57A-4A33-66CA.

Kindly help.

标签 (1)
0 项奖励
回复
16 回复数

20,431 次查看
frank_darcy
Contributor I

Do any network ports need to be open to successfully send an activation request to the remote activation server? 

0 项奖励
回复

20,426 次查看
frank_darcy
Contributor I

Ok, I think I can answer my own question. In S32DS_ARM_Installation_Guide.pdf I found this note...

Note: Make sure that TLS 1.2 protocol is enabled:
• Open Windows Control Panel > Network and Internet > Internet Options > Advanced >
Settings.
• In the Security section make sure the Use TLS 1.2 checkbox is checked. If not, check it and click
the Apply button.

So TLS implies it is a HTTPS request, presumably on the standard port 443? So if the machine has internet access working to https sites then the required port for license activation is open. I'm pretty sure TLS 1.2 is enabled by default on Ubuntu 22.04, but it can be checked. 
eg. https://support.messagemedia.com/hc/en-us/articles/4765182432399-How-to-check-if-you-re-TLS-1-2-comp...

0 项奖励
回复

22,148 次查看
amitwarbhe
Contributor I

Please provide resolution on priority, I have provided all necessary information from my end.

0 项奖励
回复

21,706 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

we met similar issues on few PC Machines - but no solution yet. The cause of the issue is Java SIGSEGV crash when calling license service, but we aren't able find reason why Java crashes. 

0 项奖励
回复

19,614 次查看
xcggg
Contributor I
Hi, I was wondering if there is any news about the solution yet. I have met the same problem on ubuntu 22.04 too. Thank you.
0 项奖励
回复

19,603 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

sorry, still no solution yet. 

0 项奖励
回复

22,133 次查看
amitwarbhe
Contributor I

Error Screenshots for installing design studio version 3.5 with activation code: A80A-6532-7AFA-413D

0 项奖励
回复

22,183 次查看
amitwarbhe
Contributor I

I am currently installing with activation code :   A80A-6532-7AFA-413D, can you please check and confirm the server registration from your end?

 

0 项奖励
回复

22,263 次查看
amitwarbhe
Contributor I

can I get the offline installer of version 3.5 with activation code:  A80A-6532-7AFA-413D

0 项奖励
回复

22,265 次查看
amitwarbhe
Contributor I

can I get the offline installer of version 3.5 with activation code:  A80A-6532-7AFA-413D

 

0 项奖励
回复

22,329 次查看
amitwarbhe
Contributor I

one of my friend is able to install with same linux version and laptop configuration

0 项奖励
回复

22,333 次查看
amitwarbhe
Contributor I

I have tried installing version 3.5 with this code as well A80A-6532-7AFA-413D, but no luck

0 项奖励
回复

22,331 次查看
jiri_kral
NXP Employee
NXP Employee

Can you please share installation log? 

0 项奖励
回复

22,327 次查看
amitwarbhe
Contributor I
no logs being generated, its getting stuck at 6%
0 项奖励
回复

22,334 次查看
amitwarbhe
Contributor I

sudo apt-get install openjdk-8-jre openjfx, this I have already done

all other linux packages which are mentioned in prerequisites

0 项奖励
回复

22,340 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

S32DS v2.2 for ARM is not tested with Ubuntu v22.04. It can be used with v20.04. Did you met the Linux installation requirements - especially Java version 8 (this version is not available on Ubuntu 22.04 by default)?

0 项奖励
回复