S32 Design Studio Extension and Update error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio Extension and Update error

ソリューションへジャンプ
3,725件の閲覧回数
avinashstarkenn
Contributor III

Screenshot 2023-08-14 151321.pngScreenshot 2023-08-14 151321.png

I am getting above error while Installing/Updating S32DS Extension for NXP's S32K3xx.

What should I do ?

 

#S32k3xx #S32DS 

 

0 件の賞賛
返信
1 解決策
3,628件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Great! Happy coding!

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,697件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @avinashstarkenn ,


There could bee possible case that server was down at the time Or internet connection broke while you were updating - installing the package. Or firewall could be blocking your request go on to the server.

Please can you try once again and see if it works.

And, if it is not resolved after trying again. 

Please can you describe problem in more detail and can you share workspace log C:\Users\Public\[workspace_name]\.metadata (or wherever your current workspace is located.

 

Thank you. Kind regards, 

 

-Mehul Patel

0 件の賞賛
返信
3,637件の閲覧回数
avinashstarkenn
Contributor III

Thank you! Issue resolved

3,629件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Great! Happy coding!

0 件の賞賛
返信