S32 Design Studio Extension and Update error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio Extension and Update error

Jump to solution
3,835 Views
avinashstarkenn
Contributor III

Screenshot 2023-08-14 151321.png

I am getting above error while Installing/Updating S32DS Extension for NXP's S32K3xx.

What should I do ?

 

#S32k3xx #S32DS 

 

0 Kudos
Reply
1 Solution
3,738 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Great! Happy coding!

View solution in original post

0 Kudos
Reply
3 Replies
3,807 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @avinashstarkenn ,


There could bee possible case that server was down at the time Or internet connection broke while you were updating - installing the package. Or firewall could be blocking your request go on to the server.

Please can you try once again and see if it works.

And, if it is not resolved after trying again. 

Please can you describe problem in more detail and can you share workspace log C:\Users\Public\[workspace_name]\.metadata (or wherever your current workspace is located.

 

Thank you. Kind regards, 

 

-Mehul Patel

0 Kudos
Reply
3,747 Views
avinashstarkenn
Contributor III

Thank you! Issue resolved

3,739 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Great! Happy coding!

0 Kudos
Reply