S32 DS install fail——rolling back

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 DS install fail——rolling back

1,829件の閲覧回数
Qingguo
Contributor I

When install S32 DS,always appear rolling back error;before Software Activation Code;pls help to solve this problem;THKS!

0 件の賞賛
返信
4 返答(返信)

1,577件の閲覧回数
hicensezhang
Contributor I

Hi, I met the rolling back problem , could you have resolve the problem?

0 件の賞賛
返信

1,807件の閲覧回数
Qingguo
Contributor I

When I  close the 360 software,it can be installed successfully!

0 件の賞賛
返信

1,824件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Qingguo,

Seems that you are attempting to install to a PC using an account which is not part of the Administrators security group. This is listed as required in the installation guide.
Please contact your IT require higher admin privileges.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,820件の閲覧回数
Qingguo
Contributor I

@Robin_Shen Thank you for your feedback;But this install was in my personal PC,and the user admin privileges!Then I try it again in admin privileges,but it always failed!

0 件の賞賛
返信