S32 DS for ARM Version 2018.R1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 DS for ARM Version 2018.R1

2,677 Views
kwakd_y
Contributor III

I installed the program to use s32k116(S32 DS for ARM Version 2018.R1).

And then updated  " S32DS_ARM_v2018.R1_UP1.zip " but the following error occurs.

What should I do?
pastedImage_1.png
0 Kudos
Reply
1 Reply

2,384 Views
mikedoidge
NXP Employee
NXP Employee

Hello kwakd.y‌,

I was unable to reproduce the issue. Could you please try to install the latest update? 

S32 Design Studio for Arm® 2018.R1 Update 8 SDK S32K1xx RTM BETA v.2.9.2

This update includes the content of all previous updates, so it is not necessary to install them separately. This may resolve your issue.

Best Regards,

Mike