S32 Check value of variables

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Check value of variables

3,180 次查看
qiaodeng
Contributor II

Hi every body,

    I can't see any variable in the variables window. I want to check the value of some variables, but when I tried  to add them to the expression window, they didn't show , and the software often encounter a problem of no response.

155429_155429.pngpastedImage_0.png

     What is the correct way to check the value of variables? Any tips would be highly appreciated.

 

Best Regards

Qiao

标签 (2)
0 项奖励
回复
3 回复数

2,667 次查看
xuantruongdao
NXP Employee
NXP Employee

Sometime this problem occurs. You can see in debugger view, it is not displayed fully. You should terminate and debug again and recheck. Hope to help you.

0 项奖励
回复

2,667 次查看
qiaodeng
Contributor II

pastedImage_0.png

    I still can't see any variable or register...Have you ever encountered this situation?

0 项奖励
回复

2,667 次查看
stanish
NXP Employee
NXP Employee

Hi,

Unfortunately S32DS cannot display/update neither a variable nor peripheral register while the target is running.

You should suspend the execution first and then check the "Expressions/EmbSysReg" Views.

Stan

0 项奖励
回复