Run a routine from ram el frame_dummy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Run a routine from ram el frame_dummy

4,598 Views
cholland
Contributor V

Hi,

I came across this post when trying to fix a problem in my design.

Home /Software Forums/ S32 Design Studio Knowledge Base/ HOWTO: Run a routine from RAM in S32 Design Studio

HOWTO: Run a routine from RAM in S32 Design Studio - NXP Community

The post mentions that the problem is fixed in the latest version of S32, but the problem still exists for me.

S32 Design Studio for Power Architecture

Version 2017.R1

Build Id 171018

 

Thanks for your help,

0 Kudos
Reply
3 Replies

4,517 Views
cholland
Contributor V

Hi,

Thanks for your reply.

I am sorry for the late reply. I was out sick.

The compiler is not being updated to the February version you posted.

I updated to version 3. 

S32 Design Studio for Power Architecture 2017.R1 Update 3 - S32Rx7x SDK EAR 0.8.3
I am still getting the Error and the gcc version remains the same.

 

I tried updating to 

S32 Design Studio for Power Architecture 2017.R1 Update 3 - S32Rx7x SDK EAR 0.8.3
Which should be the update I need, but I did not see the compiler update. 

This version mentions the gcc version 4.9.4 update, but it is a Tar ball, which I am not familiar with, so I opted for the Zip version

Compiler and Build Tools Source Package – GCC v4.9.4 for S32 Design Studio for Power Architecture® 2017.R1 Update 2(REV UP2)
Thank you,

0 Kudos
Reply

4,478 Views
cholland
Contributor V

I finally ended up giving up on trying to fix S32 Version 2017.R1 and updated to S32 Version 2.1.

I have been putting off updating S32, but this issue needed fixing.

I had to fix a few issues with the paths not pointing to the correct tools. Nothing is ever easy.

As far as S32 2017.R1, no matter what I tried upgrading to, I still got the same powerpc-eabivle-gcc version.

In conclusion, it works now.

Thank you,

0 Kudos
Reply

4,547 Views
stanish
NXP Employee
NXP Employee

Hello,

Have you installed Update 2 as recommended by Alex?

This update includes also GCC update package.

Please verify the gcc build version as depicted on the attached screenshot.

hope it help

stanish_0-1611680569790.png

 

 

0 Kudos
Reply