Problems with High DPI displays

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with High DPI displays

2,564 Views
reneherrero
Contributor I

Hi,

 

I got a shiny new Dell Precision 5510 mobile workstation with a 4k display which is marvelous.  Problem: the S32 Design Studio for ARM can't cope with the 3840 x 2160 resolution.

 

The problem is not with S32 IDE, but with the underlying Eclipse Luna (4.4.2) platform.  As you can see from the image down below, it makes the IDE pretty much unworkable.

 

Most of these scaling issues have been fixed in Eclipse Neon (still broken in Mars).

 

Any chance you guys can add this to your backlog?

 

Thanks,

 

Rene

 

158383_158383.PNGHighDpiProblem.PNG

Labels (1)
0 Kudos
Reply
2 Replies

2,435 Views
stanish
NXP Employee
NXP Employee

Hello Rene,

Thanks for pointing on this issue!

I've logged this issue into our defect tracking system under the number ENGR00381768.

Our product team can consider it in next S32DS releases.

Regards,

Stan

0 Kudos
Reply

2,435 Views
reneherrero
Contributor I

Thanks Stan.

FYI - Same is happening with the Kinetis IDE...

0 Kudos
Reply