Problem with S32 Design Studio for Power v1.2 - Update 2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with S32 Design Studio for Power v1.2 - Update 2

ソリューションへジャンプ
5,172件の閲覧回数
jobu
Contributor II

Hello,

I get some error messages if I try to install the update. Please see attached file.

Some hints to fix the problem are welcome...

Regards

Jörg

ラベル(1)
0 件の賞賛
返信
1 解決策
4,973件の閲覧回数
jobu
Contributor II

... I finally manged the update. I have disabled all URLs in "Available Software Sites" and then it works.

Jörg

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,974件の閲覧回数
jobu
Contributor II

... I finally manged the update. I have disabled all URLs in "Available Software Sites" and then it works.

Jörg

0 件の賞賛
返信
4,974件の閲覧回数
jobu
Contributor II

... I have switched off the firewall but no difference. Also my network connection is fine.

Other suggestions?

Jörg

0 件の賞賛
返信
4,974件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hello Jörg, 

I updated S32DS right now and have no issue with that. In your case it may be some temporary network outage or firewall issue on your network. If the errors are still present - check the firewall settings and network connection. 

Jiri 

0 件の賞賛
返信