Problem of the EmbSys Registers of S32D when debug the FlexPWM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem of the EmbSys Registers of S32D when debug the FlexPWM

932 次查看
pierre_theron
Contributor III


Question asked by Max Lee on Mar 21, 2018
Latest reply on Oct 14, 2019 by Pierre Theron https://community.nxp.com/community/feeds/messages?thread=472257" title="RSS

Hi,

 

I'm trying to debug the FlexPWM of MPC5744P with S32D 2017.R1, I want to see the registers about FlexPWM, so I used "EmbSys Registers" to check those registers, but I found something wrong, following pictrues shown my code and some registers:

微信图片_20180321161054.png微信图片_20180321161101.png

You can see the value of FlexPWM0_INIT_sub0 is 0xE0C0, but the value displayed by the EmbSys Registers is 0x0000, and this problem also happened on other registers which are adjacent. 

 

But the function of the code is realized, so what happened about the IDE or something else?

 

Thanks for any assistance.

 

Best regards,

Max Lee

 

Outcomes

Visibility: S32 Design Studio140 Views
Last modified on Mar 21, 2018 1:43 AM
Tags:flexpwm
Content tagged with flexpwm
S32 Design Studiompc5744p
Content tagged with mpc5744p
S32 Design Studios32ds power
Content tagged with s32ds power
S32 Design Studioembsys
Content tagged with embsys
S32 Design Studioembsysregisters
Content tagged with embsysregisters
Ratings:
Average User Rating: No ratings (0 ratings)
Average User Rating
No ratings
0
(0 ratings)
  • Comment on your rating

This content has been marked as final. Show 2 comments
Problem of the EmbSys Registers of S32D when debug the FlexPWM

Name(Required)
Email Address(Required, will not be published)
Website Address
  • Stanislav Sliva
    Mark Correct
    Correct Answer

    Hi Max,

     

    Could you try to enter a value into SUB0_INIT manually in Embsys registers View?

     

    BR,

    Stan

    Helpful Yes NoLike Show 0 Likes0 Report AbuseReply
  • Pierre Theron
    Mark Correct
    Correct Answer

    I have the same problem. It looks like an Endian problem as these registers are 16 bit and all the flexPWM registers are swopped. The processor is Big Endian, compiler and assembler is also set-up for Big Endian and the header file is Big Endian, but the alignment looks like to be Little Endian. If I write to a register manually in Embsys registers View the value changes and the value is correct if I move my mouse over the value in the code, but if the value is changed in the code it changes the wrong register.

     

    Regards,

    Pierre

0 项奖励
回复
0 回复数