Print on Debug Console

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Print on Debug Console

2,226件の閲覧回数
saad_saeed
Contributor III

Hello,

I am using a custom S32K148 . I want to debug my application using Debug Console. How would I do it. Kindly, help me with it.

Kind Regards,

Saad.

タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,088件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

answer for your question is in the thread below. My colleague Jiri explains, how to use debug console in S32DS.

Please check and let me know, if it works on your side.

https://community.nxp.com/message/1057928?commentID=1057928#comment-1057928 

Regards,

Martin

2,088件の閲覧回数
saad_saeed
Contributor III

Thankyou Martin,

Yes I tried it but problem is I am not using UART. I am programming using JTAG. 

However, I did followed what was mentioned in the post and I got the following errors

Error.PNG

0 件の賞賛
返信

2,088件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

please add -z muldef linker option into your project. Please see the thread below:

https://community.nxp.com/message/1020884?commentID=1020884#comment-1020884 

Hope this resolve the issue.

Regards,

Martin

0 件の賞賛
返信