Package for S32R45

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Package for S32R45

1,731 Views
HyunungPark
Contributor III

I installed the package like the Radar extension package and S32R45 development for S32R45 like below.

But I cannot find the BBE32 DSP Add-On Package and S32R45_RSDK_0.9.4_D2112 package for S32R45.

and I cannot find the example code for S32R45

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-New-Project-from-Example-....

Could you please give me helps?

BRs.

Hyunung Park

0 Kudos
Reply
1 Reply

1,722 Views
mikedoidge
NXP Employee
NXP Employee

Hello @HyunungPark,

The RadarSDK and the BBE32 DSP Add-On Package are premium software which available only via a special request. Please contact your local NXP Sales team or Distributor Sales team for this.

I see there is an evaluation version of the Radar SDK available on the S32R45 product page:

https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32r-radar-proc...

Best Regards,

Mike

0 Kudos
Reply