PE Micro and Digitus Network Server

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PE Micro and Digitus Network Server

2,440 Views
20Sidar04
Contributor III

Dear Mr./Mrs,

When two developer try to debug MPC5777C board by using PE Micro debugger via digitus network server, a developer couldn't debug board. What is solution for it? How is possible to debug  two different board in same time via digitus network server?

Best regards.

0 Kudos
Reply
3 Replies

2,420 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

I' not sure about your configuration. You have PE Micro begugger connected to board and USB cable is connected to Network Server USB side and Network Server is connected to PC via Ethernet cable? 

 

What particular model of Digitus Network Server do you have and which PE Micro device?

 

Jiri

0 Kudos
Reply

2,367 Views
20Sidar04
Contributor III

Dear Jiri,

Our Digitus print server model is DN-13023.

BOARD->PE Micro  Debugger-> Print Server-> Wifi->Server-> Wifi->Computer-> IDE.

Our connection is like above.

Best Regards.

 

0 Kudos
Reply

2,357 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

technically - it may work with your setup, but there is still chance that PE Micro won't work in such environment - especially if the USB to Ethernet converter is specialized for printers. You can try to reduce speed and increase delays:

jiri_kral_0-1644927153947.pngjiri_kral_0-1644927153947.png

 

PE Micro as a device is visible on target PC machine, correct? 

 

Related to debugging two boards - I'm not sure about the scenario. But you will need two probes and two instances of S32DS (on one PC or on two different PC machines). 

 

0 Kudos
Reply