P&E problem in S32 evironment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P&E problem in S32 evironment

1,348 Views
朱先生
Contributor III

Hi, 

I use P&E to debug our source code(The mcu is MPC5744P, the version of S32 is 1.2). 

When I pressed the debug button, connection error would be pop up. The sequence is shown below:

step 1: shown confirm window. I press "Yes" button.

pastedImage_1.png

step 2: P&E connection assistant window. I press "Retry" button.

pastedImage_2.png

step 3: need power cycle.  Then I power down the target and press "OK"

pastedImage_3.png

step 4: unknown information.  

pastedImage_4.png

In "Console" window, some error are list below:

pastedImage_5.png

so, how I can solve this issue? Thank you.

Bryce

0 Kudos
Reply
0 Replies