Multiple Hardware configuration for S32K34 in S32DS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Multiple Hardware configuration for S32K34 in S32DS

跳至解决方案
1,424 次查看
HemantK
Contributor III

Hello, 

 

We have two hardware board based on S32K3 and they have different CAN Pin settings. 

So I created one project with two different functional groups 'VS_0' and 'VS-1' but when I generate the code it includes both groups code and thus when I compile it, it gives linker error as follows: 

c:/nxp/s32ds.3.4/s32ds/build_tools/gcc_v10.2/gcc-10.2-arm32-eabi/bin/../lib/gcc/arm-none-eabi/10.2.0/../../../../arm-none-eabi/bin/real-ld.exe: ./generate/src/FlexCAN_Ip_Sa_VS_1_PBcfg.o:C:\xbms\xbms_application\Application\Debug_FLASH/../generate/src/FlexCAN_Ip_Sa_VS_1_PBcfg.c:107: multiple definition of `FlexCAN_State0'; ./generate/src/FlexCAN_Ip_Sa_VS_0_PBcfg.o:C:\xbms\xbms_application\Application\Debug_FLASH/../generate/src/FlexCAN_Ip_Sa_VS_0_PBcfg.c:107: first defined here
c:/nxp/s32ds.3.4/s32ds/build_tools/gcc_v10.2/gcc-10.2-arm32-eabi/bin/../lib/gcc/arm-none-eabi/10.2.0/../../../../arm-none-eabi/bin/real-ld.exe: ./generate/src/FlexCAN_Ip_Sa_VS_1_PBcfg.o:C:\xbms\xbms_application\Application\Debug_FLASH/../generate/src/FlexCAN_Ip_Sa_VS_1_PBcfg.c:110: multiple definition of `FlexCAN_State1'; ./generate/src/FlexCAN_Ip_Sa_VS_0_PBcfg.o:C:\xbms\xbms_application\Application\Debug_FLASH/../generate/src/FlexCAN_Ip_Sa_VS_0_PBcfg.c:110: first defined here

 

Can you please guide me as what I am doing wrong.

 

Regards, 

Hemant Kapoor

0 项奖励
回复
1 解答
1,408 次查看
HemantK
Contributor III

Thanks for the response...

 

The way I got round this issue is by excluding the unwanted file from the project.

But there are still some issues with the supporting multiple hardware in the IDE

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,411 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @HemantK 

Unfortunately, the functional groups feature of the S32 Configuration Tools is not fully supported by the PlatformSDK_S32K3_2022_xx_S32K34x_M7 SDK (installed within S32DS as part of the S32K3 Real-Time Drivers package). This is why you are seeing these errors. Most likely, you will need to create 2 separate projects. If you want to keep some of the files shared across the 2 projects, so they could more easily be kept in sync, you might consider either using linked files or maintaining some portion as a library project.

Best Regards,

Mike

0 项奖励
回复
1,409 次查看
HemantK
Contributor III

Thanks for the response...

 

The way I got round this issue is by excluding the unwanted file from the project.

But there are still some issues with the supporting multiple hardware in the IDE

0 项奖励
回复