Missing status.h header file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing status.h header file

Jump to solution
4,517 Views
ArkAndyFraser
Contributor III

I have a simple board with a S32K144W (48-pin) and am trying to create a very simple application using S32 Design Studio. I used the Config Tools to setup the main system clocks, SWD, Low Power Timer and Low Power UART. I generated all the code for the above configuration however, when I build the project I get:

fatal error: status.h: No such file or directory

This file is referenced by the peripheral header files.

Can anyone help?

Andy

0 Kudos
Reply
1 Solution
4,458 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ArkAndyFraser 

Some irregularities have been reported by other customers about the support of S32K1 devices with S32DS v3.5. 

Please help us use S32DS3.4 for these devices. And let us know if the problem persists. 

View solution in original post

5 Replies
4,489 Views
ArkAndyFraser
Contributor III

@VaneB 

I used the Update Code button before building.

Please find additional information below.

S32 Design Studio for S32 Platform
Version: 3.5
Build id: 230728 (Update 4)

ArkAndyFraser_0-1693336088139.png

ArkAndyFraser_1-1693336213891.png

 

Hope this helps.

Andy

0 Kudos
Reply
4,459 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ArkAndyFraser 

Some irregularities have been reported by other customers about the support of S32K1 devices with S32DS v3.5. 

Please help us use S32DS3.4 for these devices. And let us know if the problem persists. 

4,411 Views
ArkAndyFraser
Contributor III
@VaneB
Yes, dropping back to 3.4 seems to have done the trick. I hope NXP is working on this as I don't like running older versions of development tools.

Andy
3,206 Views
mstroven
Contributor III

Since this was posted over a year ago, I expected that NXP would have fixed this issue by now, but unfortunately, it still persists in S32DS 3.5.  What's the deal, guys?

0 Kudos
Reply
4,493 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ArkAndyFraser 

Could you provide me with the following information?

  • IDE version 
  • SDK/RTD version 
  • configurations made 
  • Once you made the configurations, did you update the code?

The more details you provide us on the steps you made to create and implement the project, It is easy for us to understand the problem.

 

B.R.

VaneB

0 Kudos
Reply