Missing status.h header file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing status.h header file

ソリューションへジャンプ
4,482件の閲覧回数
ArkAndyFraser
Contributor III

I have a simple board with a S32K144W (48-pin) and am trying to create a very simple application using S32 Design Studio. I used the Config Tools to setup the main system clocks, SWD, Low Power Timer and Low Power UART. I generated all the code for the above configuration however, when I build the project I get:

fatal error: status.h: No such file or directory

This file is referenced by the peripheral header files.

Can anyone help?

Andy

0 件の賞賛
返信
1 解決策
4,423件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @ArkAndyFraser 

Some irregularities have been reported by other customers about the support of S32K1 devices with S32DS v3.5. 

Please help us use S32DS3.4 for these devices. And let us know if the problem persists. 

元の投稿で解決策を見る

5 返答(返信)
4,454件の閲覧回数
ArkAndyFraser
Contributor III

@VaneB 

I used the Update Code button before building.

Please find additional information below.

S32 Design Studio for S32 Platform
Version: 3.5
Build id: 230728 (Update 4)

ArkAndyFraser_0-1693336088139.png

ArkAndyFraser_1-1693336213891.png

 

Hope this helps.

Andy

0 件の賞賛
返信
4,424件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @ArkAndyFraser 

Some irregularities have been reported by other customers about the support of S32K1 devices with S32DS v3.5. 

Please help us use S32DS3.4 for these devices. And let us know if the problem persists. 

4,376件の閲覧回数
ArkAndyFraser
Contributor III
@VaneB
Yes, dropping back to 3.4 seems to have done the trick. I hope NXP is working on this as I don't like running older versions of development tools.

Andy
3,171件の閲覧回数
mstroven
Contributor III

Since this was posted over a year ago, I expected that NXP would have fixed this issue by now, but unfortunately, it still persists in S32DS 3.5.  What's the deal, guys?

0 件の賞賛
返信
4,458件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @ArkAndyFraser 

Could you provide me with the following information?

  • IDE version 
  • SDK/RTD version 
  • configurations made 
  • Once you made the configurations, did you update the code?

The more details you provide us on the steps you made to create and implement the project, It is easy for us to understand the problem.

 

B.R.

VaneB

0 件の賞賛
返信