MPC5748G: S32 software debug can not write in

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5748G: S32 software debug can not write in

1,785 次查看
he_zhang
Contributor I

IMG_20191106_184949.jpg

Loading programming algorithm . . .

WARNING - Selected .PCP file has been modified. CRC16 = $5A63

Done.

Programming sequency is : erase, blank check, program, and verify { default }

CMD>VC

Verifying object file CRC-16 to device ranges . . .

      block 00F90000-00F9001B  . . .

 

 

When using software debug debugging, the code is written, the card is 99%, the above is the log, it seems that the chip can not be erased? Is the sector damaged?

After I replaced the MPC5748G chip, I can debug it. . .

0 项奖励
回复
3 回复数

1,639 次查看
he_zhang
Contributor I

Yes! Can you guess the cause of this problem? Or can you provide a direction for the investigation?

thank you very much!

0 项奖励
回复

1,639 次查看
jiri_kral
NXP Employee
NXP Employee

Hi,

Well, you can try to use RAM Target project and check registers or just attach to running target and try to figure out what's wrong. You can also try to update OpenSDA firmware - https://community.nxp.com/docs/DOC-340263  

Jiri

0 项奖励
回复

1,639 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

it's hard to say what's wrong - but as you said - the issue is with chip. With other MCU it is working, correct? 

Jiri 

0 项奖励
回复