MPC5744P can not debug with PE Multilink universal debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P can not debug with PE Multilink universal debugger

2,342件の閲覧回数
1067929469
Contributor I

Hi NXP:

I have two boards of we own designed, In the beginning, two boards can debug with PE Multilink universal debugger, I dont't know what happened, Now one board can not dubug with PE Multilink universal debugger,the fault message tips in the following figure:

微信截图_20200819140208.png

0 件の賞賛
返信
2 返答(返信)

2,276件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

You might censor the board if you program a DCF record into DFLASH as indicated by Lukas.

Anyway if you can connect and debug one board only, it may indicate probably a hw issue with the other board.

Please check:

* Pemicro probe LEDs (blue, yellow) are ON when the board is powered up?

* is there a reasonable power consumption when you power up the board. Please check the power supply voltages for MCU

* Boot mode signals (FAB/ ABS) set to boot from internal flash?

* can check if crystal clock is oscillating and

* state of the RESET line (as suggested by Lucas)

hope it helps...

Stan

0 件の賞賛
返信

2,276件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

did you check the reset line? Is it deasserted after power on?

Did you touch censorship information or DCF records before that?

Regards,

Lukas

0 件の賞賛
返信