MPC5744 Debug error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744 Debug error

2,697件の閲覧回数
dsytj88
Contributor II

Version:S32 v1.2

after flashing the file into MCU.I tried to use debug mode to lauch MPC5744P.elf file,

in the progress it will be blocked,and error box appeared:

Error with command: gdb --version
Cannot run program "gdb": Launching failed

I tried another demo and it shows the same problem,do you know what's the reason and how to resolve it?

thank you

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

2,175件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

Could you possibly check if the debug configuration is complete.

pastedImage_1.png

I'd also recommend you to try to create a new workspace in  v1.2 and import your project.

Hope it helps.

Stan 

0 件の賞賛
返信