MAC57D5xxEVB Flashx Example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MAC57D5xxEVB Flashx Example

1,306 次查看
ydbae78
Contributor I

-. Target Board : MAC57DxxEVB

-. Using IDE : S32DS

-. Debugging Tool : PE micro multilink-fx

-. External Flash : Micron Nor Flash (with QSPI1) 

Question : I want to write and read image data in external flash memory.

                 Can I have document or example code to refer to?

The world is in a difficult situation, but I hope everyone is healthy.

标签 (1)
标记 (4)
0 项奖励
回复
1 回复

1,195 次查看
ankur_kala
NXP Employee
NXP Employee

QSPI controller is described in the device RM. Also, attached is the QSPI example based on S32DS IDE. The example writes a fixed data on a section of QSPI flash. The same can be modified as per user requirement.

0 项奖励
回复