MAC57D5xxEVB Flashx Example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MAC57D5xxEVB Flashx Example

1,887件の閲覧回数
ydbae78
Contributor I

-. Target Board : MAC57DxxEVB

-. Using IDE : S32DS

-. Debugging Tool : PE micro multilink-fx

-. External Flash : Micron Nor Flash (with QSPI1) 

Question : I want to write and read image data in external flash memory.

                 Can I have document or example code to refer to?

The world is in a difficult situation, but I hope everyone is healthy.

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

1,776件の閲覧回数
ankur_kala
NXP Employee
NXP Employee

QSPI controller is described in the device RM. Also, attached is the QSPI example based on S32DS IDE. The example writes a fixed data on a section of QSPI flash. The same can be modified as per user requirement.

0 件の賞賛
返信