Linked files not found by compiler?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Linked files not found by compiler?

跳至解决方案
6,997 次查看
gearhead1107
Contributor IV

When I use this guide to create linked files in S32DS, I use Ctrl+click/drag to take one file "CAN_TxRx.h" and move it into another project, linked relative to "PROJECT_LOC", however it seems the compiler cannot "see" the linked file

In the build for this project, I get the following error:

../Sources/CAN_TxRx.c:8:22: fatal error: CAN_TxRx.h: No such file or directory

..even though the file appears in the "include" folder as a linked file.

I've searched around, and most of the issues relate to folks not adding another project's path to the compiler's include path - which doesn't sound relevant to this issue, since the project builds with no errors when "CAN_TxRx.h" is copied in the file system.

Is there a build setting I should look for that excludes linked files?

0 项奖励
回复
1 解答
5,638 次查看
stanish
NXP Employee
NXP Employee

Andrew, 

Can you post here the "CAN_TxRx.args" file. This file should be located somewhere in your output directory e.g. "Debug\Sources". It contains all the include paths. 

Drag&Drop a header file as a linked file into your project does not add the include path into your project properties. You have to do it manually e.g. here:

pastedImage_3.png

or here:

pastedImage_4.png

Hope it helps.

Stan

在原帖中查看解决方案

0 项奖励
回复
4 回复数
5,637 次查看
gearhead1107
Contributor IV

It's a bummer that you have to manually go back and include the path when the "feature" should supposedly make it seamless.

Ironically it seems that both must be done - c files must be virtually added to the build path, and includes must be specified under paths and symbols

0 项奖励
回复
5,637 次查看
BlackNight
NXP Employee
NXP Employee

Is this error generated by the compiler? What happens is that the 'make' (or managed make) driver callse the compiler with the source (*.c) file and passes the option -I to the compiler with the search path list where to find the header file. It seems to me that the compiler cannot find that header file. Can you double check that the -I option has the path to that CAN_TxRx.h file present? For testing you might specify he absolute path to that directory too in the compiler settings.

I hope this helps,

Erich

0 项奖励
回复
5,637 次查看
gearhead1107
Contributor IV

Hey Erich! The path for both the linked and non-linked version of the file is the following:

"${ProjDirPath}/include"

0 项奖励
回复
5,639 次查看
stanish
NXP Employee
NXP Employee

Andrew, 

Can you post here the "CAN_TxRx.args" file. This file should be located somewhere in your output directory e.g. "Debug\Sources". It contains all the include paths. 

Drag&Drop a header file as a linked file into your project does not add the include path into your project properties. You have to do it manually e.g. here:

pastedImage_3.png

or here:

pastedImage_4.png

Hope it helps.

Stan

0 项奖励
回复