Install S32DS on Windows without using built-in Java

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Install S32DS on Windows without using built-in Java

跳至解决方案
2,816 次查看
Manuel314
Contributor II

Hello cummulity,

In my company the IT is blocking the use of Oracle Java for security reasons. They have provided us all with an alternative build of Java that is installed on all our computers.

I now want to install S32DS on my windows 11 machine, but want to use the JRE that is already available on the computer.

I have found that the S32DS installer always tries to run the JRE that is included in the installer package and is then blocked by our firewall and I can't install it.

Since the installer package for Linux does not include a JRE, is there such an option for windows as well?

 

Thanks

标记 (3)
0 项奖励
回复
1 解答
2,431 次查看
Manuel314
Contributor II

I have found sort-of a solution together with our IT-department. My issue exactly is, that only Oracle-Java is blocked. The newer versions of S32DS don't use Oracle Java (like 3.4, which we are using) anymore but OpenJDK. A solution would be to simply update to the newest version.

In our particular case that is not an easy option since our project relies on features that 3.4 has and 3.5up does not support anymore.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,766 次查看
Manuel314
Contributor II

I'm searching for an option to have a (Windows 11 -) installer for S32DS without JRE (similar to the one for Linux). Maybe some of the NXP-staff?

 

Thank you in advance

0 项奖励
回复
2,742 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can specify java vm in s32ds.ini file (located in c:\NXP\S32DS.3.6.0\eclipse\  folder) once S32DS is installed. But windows installer itself uses build in java vm. 

0 项奖励
回复
2,737 次查看
Manuel314
Contributor II

Hi,

that is the very problem I'm facing. I can't run the installer, because it uses the build-in java vm.

Since the installer for Linux does not, I asked myself, if something similar would be available for windows.

0 项奖励
回复
2,448 次查看
scallaway21
Contributor I

Has there been any update to this? I am facing the same issue.

0 项奖励
回复
2,432 次查看
Manuel314
Contributor II

I have found sort-of a solution together with our IT-department. My issue exactly is, that only Oracle-Java is blocked. The newer versions of S32DS don't use Oracle Java (like 3.4, which we are using) anymore but OpenJDK. A solution would be to simply update to the newest version.

In our particular case that is not an easy option since our project relies on features that 3.4 has and 3.5up does not support anymore.

0 项奖励
回复