Import and copy project from command line (Win)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Import and copy project from command line (Win)

2,170件の閲覧回数
Catosh
Contributor IV

Hello, 

I need to import and copy into a workspace an existing project using command line. 

Usual approach with 

s32ds.exe -nosplash -data path-to-workspace -application org.eclipse.cdt.managedbuilder.core.headlessbuild -import {[uri:/path-to-project}

returns a lot of errors: 

pastedImage_3.png

I can see in the help file that s32DS studio uses other plugins, but I suppose they are only used for processor expert related operations.

Command Line Interface

com.freescale.processorexpert.core.PExApplication

How can I import projects in a new workspace (and copy them into)using command line?

 

Thanks and B.R.

L.

タグ(3)
0 件の賞賛
返信
0 返答(返信)