IPCF - communicating between M core and A-Core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IPCF - communicating between M core and A-Core

2,037 Views
ggowdar
Contributor I

Hi Team,

               I am using the IPCF 2.1.1 and able to send data from A-core to M-core by following the IPCF user manual. 

just wondering how can I transfer data from M-core to A-core, currently I see from the user manual the procedure is for only A-core to M-core and check on the reply/echo messages.

is there any option to send a message from M-core to A-core in the same way as it is provided from A-core to M-core.

I am using S32G EVB board.

Appreciate your quick reply.

Thank You

0 Kudos
Reply
1 Reply

2,020 Views
bpe
NXP Employee
NXP Employee

The procedure that sends an echo response in the available demo application for the M7 side is pretty generic and can be used independently of the incoming communication provided that the payload is generated locally instead of copying it from the received message.

 

Best Regards,
Platon

0 Kudos
Reply