IAR Embedded Workbench Eclipse Plugin Problem In S32DS for ARM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IAR Embedded Workbench Eclipse Plugin Problem In S32DS for ARM

2,466 Views
zhiwei1
Contributor I

Ask for help

I tried to configure IAR Plugin and encountered the following problems:

zhiwei1_0-1651197544828.pngzhiwei1_0-1651197544828.png

 

0 Kudos
Reply
3 Replies

2,433 Views
mikedoidge
NXP Employee
NXP Employee

Hi Zihwei,

It looks like the IAR plugin is requiring some Eclipse package which did not exist when S32 Design Studio for Arm was released. You will need to locate this package from http://download.eclipse.org site and install it.

Best Regards,

Mike

0 Kudos
Reply

2,387 Views
zhiwei1
Contributor I

Hi Mike,

What is the specific download address of "package org.eclipse.jdt.internal.eval 0.0.0",For example.When I need to download EMF, the download address is http://download.eclipse.org/modeling/emf/emf/builds/release/2.13.

0 Kudos
Reply

2,380 Views
mikedoidge
NXP Employee
NXP Employee

Hello Zhiwei,

Probably you should contact IAR for this information. It's possible the package is standard one on newer versions of Eclipse. You might want to check the release notes for the IAR plug-in to see which versions of Eclipse are supported. It's possible it is for a new version of Eclipse than the one you have installed with S32 Design Studio for Arm. Probably IAR could guide you to the correct plug-in version for the IAR compiler you wish to use and for the Eclipse version included with the S32 Design Studio for Arm version you've chosen.

Best Regards,

Mike

0 Kudos
Reply