How to view the call hierarchy When using the S32Studio tool to debug ELF files generated by greenhills

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to view the call hierarchy When using the S32Studio tool to debug ELF files generated by greenhills

2,614 Views
331447791
Contributor I

build and link environment:  greenhill  comp_201714

build cmd : -cpu=cortexm4 -noobj --long_long -G -dual_debug -farcalls -dwarf2 -no_misalign_pack -nostartfiles

S32 Design Studio version: 

Version: 2018.R1
Build id: 180326

I used greenhill to build and generated elf file.  when debug with elf file and open call hierarchy window I always see that.  how the view the call hierarchy?

pastedImage_2.png

Labels (1)
0 Kudos
Reply
4 Replies

2,445 Views
stanish
NXP Employee
NXP Employee

Hi, 

Could you try to re-index the project:

pastedImage_2.png

Stan

0 Kudos
Reply

2,445 Views
331447791
Contributor I

Hi  Stanislav:

I have try to Index rebuild operation. but still can not  view the call hierarchy. S32 Design Studio did not anything when executing index rebuild operation .   Do Must use the S32 Design Studio build source and then to executing  this operation?

0 Kudos
Reply

2,445 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

what is your target MCU? 

Jiri

0 Kudos
Reply

2,445 Views
331447791
Contributor I

S32K148

0 Kudos
Reply