How to turn off file comparison window

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to turn off file comparison window

ソリューションへジャンプ
2,771件の閲覧回数
zp001
Contributor III

Hello,

There is a pop-up window while updating code. I have to click "ok" buttion for each file.

screenshot as below

zp001_0-1669720456304.png

I'd like to know how to turn off this option.

Thanks!

0 件の賞賛
返信
1 解決策
2,707件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi Zhend,

I believe I discovered the problem. You are using S32 Design Studio for S32 Platform v3.5 and you have somehow managed to install onto it the following:

RTD S32K3XX 2.0.1.202207071057 com.nxp.RTD.S32K3XX.root.2.0.1.feature.feature.group NXP Semiconductors, Inc.
RTD S32K3XX 2.0.1 2.0.1.202207071057 com.nxp.RTD.S32K3XX.2.0.1.feature.feature.group NXP Semiconductors, Inc.

These packages do not support S32DS 3.5, they were developed for and tested to S32DS 3.4 Update 3. They are not forward compatible.

If you wish to use this RTD package, then please install it onto the S32DS v3.4. I also highly recommend that you use the S32DS Extensions and Updates menu to install as it has built-in dependency checking and would have prevented this incorrect configuration.

Best Regards,

Mike

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
2,719件の閲覧回数
zp001
Contributor III

Hi Mike,

I also found some abnormal things that there were always some modules could't be loaded successfully. I hadto add them one by one.

Even through the project can be build normally after that, It's weired a little bit,but I don't know why.

scrreenshot as below:

zp001_0-1669950477108.png

 

0 件の賞賛
返信
2,745件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello,

This is not normal behavior. There is no setting to cause this. The comparison window should only appear when a comparison is performed, not from Update Code command.

Could you please share the file '{workspace_path}\.metadata\.log'? It should contain some clues regarding what is happening.

Best Regards,

Mike

0 件の賞賛
返信
2,735件の閲覧回数
zp001
Contributor III

Hi Mike,

Thank you for your help!

I tried to re-install S32DS, but without success. 

Here is the meta log.

 

タグ(1)
0 件の賞賛
返信
2,721件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi Zhend,

Thank you for sending this information. It is looking like it could be a configuration issue. I think perhaps you are missing some package or a package did not install properly. Could you please provide the following:

Help -> S32DS Extensions and Updates, then click 'Installation Details' (blue linked text in bottom of Overview Details panel. Please send the text that is provided in the Installation Details window.

Best Regards,

Mike

0 件の賞賛
返信
2,717件の閲覧回数
zp001
Contributor III

Hi Mike,

Please see the attachment.

Thanks!

0 件の賞賛
返信
2,708件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi Zhend,

I believe I discovered the problem. You are using S32 Design Studio for S32 Platform v3.5 and you have somehow managed to install onto it the following:

RTD S32K3XX 2.0.1.202207071057 com.nxp.RTD.S32K3XX.root.2.0.1.feature.feature.group NXP Semiconductors, Inc.
RTD S32K3XX 2.0.1 2.0.1.202207071057 com.nxp.RTD.S32K3XX.2.0.1.feature.feature.group NXP Semiconductors, Inc.

These packages do not support S32DS 3.5, they were developed for and tested to S32DS 3.4 Update 3. They are not forward compatible.

If you wish to use this RTD package, then please install it onto the S32DS v3.4. I also highly recommend that you use the S32DS Extensions and Updates menu to install as it has built-in dependency checking and would have prevented this incorrect configuration.

Best Regards,

Mike

0 件の賞賛
返信
2,694件の閲覧回数
zp001
Contributor III

Hi Mike,

There is another way to fix that by deleting .metadata dirctory.

Thanks!

0 件の賞賛
返信