How to turn off file comparison window

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to turn off file comparison window

跳至解决方案
2,768 次查看
zp001
Contributor III

Hello,

There is a pop-up window while updating code. I have to click "ok" buttion for each file.

screenshot as below

zp001_0-1669720456304.png

I'd like to know how to turn off this option.

Thanks!

0 项奖励
回复
1 解答
2,704 次查看
mikedoidge
NXP Employee
NXP Employee

Hi Zhend,

I believe I discovered the problem. You are using S32 Design Studio for S32 Platform v3.5 and you have somehow managed to install onto it the following:

RTD S32K3XX 2.0.1.202207071057 com.nxp.RTD.S32K3XX.root.2.0.1.feature.feature.group NXP Semiconductors, Inc.
RTD S32K3XX 2.0.1 2.0.1.202207071057 com.nxp.RTD.S32K3XX.2.0.1.feature.feature.group NXP Semiconductors, Inc.

These packages do not support S32DS 3.5, they were developed for and tested to S32DS 3.4 Update 3. They are not forward compatible.

If you wish to use this RTD package, then please install it onto the S32DS v3.4. I also highly recommend that you use the S32DS Extensions and Updates menu to install as it has built-in dependency checking and would have prevented this incorrect configuration.

Best Regards,

Mike

在原帖中查看解决方案

0 项奖励
回复
7 回复数
2,716 次查看
zp001
Contributor III

Hi Mike,

I also found some abnormal things that there were always some modules could't be loaded successfully. I hadto add them one by one.

Even through the project can be build normally after that, It's weired a little bit,but I don't know why.

scrreenshot as below:

zp001_0-1669950477108.png

 

0 项奖励
回复
2,742 次查看
mikedoidge
NXP Employee
NXP Employee

Hello,

This is not normal behavior. There is no setting to cause this. The comparison window should only appear when a comparison is performed, not from Update Code command.

Could you please share the file '{workspace_path}\.metadata\.log'? It should contain some clues regarding what is happening.

Best Regards,

Mike

0 项奖励
回复
2,732 次查看
zp001
Contributor III

Hi Mike,

Thank you for your help!

I tried to re-install S32DS, but without success. 

Here is the meta log.

 

标记 (1)
0 项奖励
回复
2,718 次查看
mikedoidge
NXP Employee
NXP Employee

Hi Zhend,

Thank you for sending this information. It is looking like it could be a configuration issue. I think perhaps you are missing some package or a package did not install properly. Could you please provide the following:

Help -> S32DS Extensions and Updates, then click 'Installation Details' (blue linked text in bottom of Overview Details panel. Please send the text that is provided in the Installation Details window.

Best Regards,

Mike

0 项奖励
回复
2,714 次查看
zp001
Contributor III

Hi Mike,

Please see the attachment.

Thanks!

0 项奖励
回复
2,705 次查看
mikedoidge
NXP Employee
NXP Employee

Hi Zhend,

I believe I discovered the problem. You are using S32 Design Studio for S32 Platform v3.5 and you have somehow managed to install onto it the following:

RTD S32K3XX 2.0.1.202207071057 com.nxp.RTD.S32K3XX.root.2.0.1.feature.feature.group NXP Semiconductors, Inc.
RTD S32K3XX 2.0.1 2.0.1.202207071057 com.nxp.RTD.S32K3XX.2.0.1.feature.feature.group NXP Semiconductors, Inc.

These packages do not support S32DS 3.5, they were developed for and tested to S32DS 3.4 Update 3. They are not forward compatible.

If you wish to use this RTD package, then please install it onto the S32DS v3.4. I also highly recommend that you use the S32DS Extensions and Updates menu to install as it has built-in dependency checking and would have prevented this incorrect configuration.

Best Regards,

Mike

0 项奖励
回复
2,691 次查看
zp001
Contributor III

Hi Mike,

There is another way to fix that by deleting .metadata dirctory.

Thanks!

0 项奖励
回复