How to solve the problem that example project can't be compiled?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to solve the problem that example project can't be compiled?

3,887 次查看
abcb
Contributor I
Hi everyone,
After I install S32DS.ARM.2018.R1, I install RTM SDK 3.0.0 online. And then download and install "S32 Design Studio for ARM v2018.R1 Update 11 with S32 SDK S32K1xx SR 3.0.2". Create the example project (Can_pal_s32k144),
I encounter the following problems:
1. No "Cross Settings" in C/C++ Build option
2. gcc is not found
Related pictures are as below:
1. No Cross SettingsCross Setting.jpg
2. Gcc path is specofied
gcc path.jpg
3. Example Project has errors
Example  Project.jpg
Thank You
标记 (4)
0 项奖励
回复
4 回复数

3,697 次查看
happybaby8882
Contributor I

I encountered the similar problem, create a new project, generate code from PE, and build, then a lot of problems occur, probably the generated code is empty, but i don't know why.

0 项奖励
回复

3,753 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

actually I never saw such issue before. I tried reproduce it, but on my machine everything works okay. So, you can try uninstall and install S32DS again - if you require this old version.  

The latest S332DS version is - https://community.nxp.com/docs/DOC-345517 

Jiri 

0 项奖励
回复

3,753 次查看
abcb
Contributor I

Hi Jiri,

I've tried uninstall and install S32DS again, but the result is still the same.

Now I'm trying to install the latest S332DS version, hope there will be good news...

Thank you.

Adam Chiu

0 项奖励
回复

3,753 次查看
18062294269
Contributor I

hi

   I have the same problem ,have you    solved it ?

0 项奖励
回复