How to solve Processor Expert Problem - ERROR: Unexpected status of script

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to solve Processor Expert Problem - ERROR: Unexpected status of script

1,718 Views
chen1834
Contributor I

Hi all, 

My project meet a PE problem.

It reports errors as:

ERROR: Unexpected status of script: Beans\tcpip\tcpip_update.chg, please contact Freescale support.

Generator: ERROR: There are errors in the project, please review components configuration. It is not possible to generate code.

 

The SDK version I use is S32_SDK_MPC574xx_RTM_1.0.0.

I can see something strange in tcpip_middleware in the Components view, which is the lwIP version is null.null.null and wolfSSL version is 'not available'.

Normally in a correct project the lwIP version is 2.0.2 and wolfSSL version is "3.12.0".

incorrect.png

correct.png

 

What's the reason for this error? How to fix it?

 

Thanks,

 

0 Kudos
Reply
1 Reply

1,699 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

not sure what the problem is, but version RTM 1.0.0 is quite old, there's already RTM 3.0.3. So, I would try to update it as a first step.

Regards,

Lukas

 

 

0 Kudos
Reply