How to set S32DS debug to flash?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to set S32DS debug to flash?

8,768件の閲覧回数
文辉王
Contributor III

Dear all,

There is a question that needs to be consulted. I am debugging mpc5744p, but I found that when using S32DS, the code can only be downloaded to RAM, but not flash. That is to say, I can run the program when I debug, but after the dug, I find that the program is not burned in the chip. How can I solve this?

Thanks.

ラベル(1)
タグ(3)
0 件の賞賛
返信
6 返答(返信)

8,541件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can add new configuration in configuration manager: 

pastedImage_1.png

The difference between RAM and FLASH target is in Linker file. For your new configuration select linker script file for Flash target - pastedImage_2.png 

As a reference you can look at any example - almost all of them have both configurations (FLASH,RAM).

Hope it helps.

Jiri . 

0 件の賞賛
返信

8,541件の閲覧回数
文辉王
Contributor III

Hello Jiri ,

Followed your method, but it still doesn't seem to download the code to the chip.

Thanks.

0 件の賞賛
返信

8,541件の閲覧回数
stanish
NXP Employee
NXP Employee

Vern,

could you please post the debugger screen that indicates the executable has not been programmed into flash.

Please also check the debugger GDB serverv console - it should include information about the programmed sections and addresses.

pastedImage_1.png

Stan

0 件の賞賛
返信

8,541件の閲覧回数
文辉王
Contributor III

Hello Stan,

The following is the console information:pastedImage_1.png

The following is the debugger console information:

pastedImage_2.png

Thanks.

0 件の賞賛
返信

8,541件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

from you screenshot it is obvious that your program is uploaded into Flash (and already present in Flash). There is probably some error in your project - it looks that you program ends in some exception. It is possible share your project? 

Jiri 

0 件の賞賛
返信

5,294件の閲覧回数
NancyW
Contributor I

Hello, I have the same problem, i'm trying to run an existing project on S32G3 by debugging it by using Flash. I followed the steps to add the flash linker path but I couldn't find it so I add it my self, but it don't seems to be the solution because only the RAM linker is there.

Could you help me please or tell me where to find this linker to process Flash debuging ?

Thanks : )

0 件の賞賛
返信